Press Release
Back to Press Room
Diodes Incorporated Announces Next Generation DBS Product Family
DALLAS, Feb 04, 2010 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq:DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, announced the introduction of a new family of low noise block (LNB) controllers for direct broadcast satellite (DBS) applications. In smaller packaging and operating at lower voltages and higher levels of accuracy than previous generations, six new devices aim to increase efficiency and the reliability of LNB designs while reducing overall size.
These next generation controllers have proven in some cases to use less than 1% of total LNB current; their low supply voltage operation ensures a significant efficiency improvement when used with DC-DC converters. Packaging is now ultra thin QFN style, enabling a reduction in PCB size and off-board height requirement.
Offering more accurate and flexible control and internal filtering, the new controllers completely eliminate false switching and support a wider range of set-top box designs and specifications. The six controllers have been designed to exceed the latest DBS broadcast specifications.
The ZNBG3118 provides bias control and protection for up 3 GaAs and HEMT FET low noise amplifiers. This controller integrates an accurate voltage detector for LNB polarization channel selection and an advanced tone detector for local oscillator selection for band switching.
ZABG4002 and ZABG6002 are low power fixed bias controllers for 4 and 6 stage FET low noise amplifiers, respectively, providing each FET with an independent protected negative gate voltage and positive drain voltage with user programmable drain current selectable from 0 to 15mA.
Offering a choice of high and standard accuracy polarization voltage detection are the ZLNB2015 and ZLNB2016 advanced DBS dual voltage and tone detectors. Optimized for low supply current and wide operating voltage, both devices also offer excellent interference rejection while keeping application cost down.
Finally, the ZLNB254 is a dual channel DiSEqC(TM) interface for LNBs and satellite distribution systems. This IC provides two highly accurate DiSEqC detectors, which converts the DiSEqC(TM) signals into logic level representations enabling simple and reliable processor monitoring. More information on all the new LNB devices is at http://www.diodes.com/dbs.
About Diodes Incorporated
Diodes Incorporated (Nasdaq:DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, serving the consumer electronics, computing, communications, industrial and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, amplifiers and comparators, Hall-effect sensors and temperature sensors, power management devices including LED drivers, DC-DC switching regulators, linear voltage regulators and voltage references, along with special function devices including USB power switch, load switch, voltage supervisor and motor controllers. The Company's corporate headquarters and logistics office are located in Dallas, Texas. A sales, marketing, and engineering office is located in Westlake Village, California. Design centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester; with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse and logistics offices are located in Taipei; Hong Kong; Manchester and Munich, Germany, with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
972-385-2810
pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
949-224-3874
lsievers@sheltongroup.com