Press Release
Back to Press Room
Diodes Incorporated's Logic Family Saves Space with 1mm Square Package
DALLAS, Jan 20, 2011 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today announced its release of 8 single gate logic functions in the miniature 6-pin DFN1010 package. Measuring just 1.0mm by 1.0mm and with a maximum off-board height of 0.4mm, the latest additions to the 74LVC1Gxx logic family provide space-saving opportunities for the smallest handheld devices, including advanced cell phones, satellite navigation systems and tablet computers.
The product introduction includes 3-input NAND and 3-input AND gates and four configurable multifunction gates providing a choice of up to 7 different logic functions each. A Schmitt trigger inverter and Schmitt trigger buffer complete the new offerings, all of which are all also being made available in industry standard SOT packaging.
The logic devices' wide operating voltage range of 1.65V to 5.5V means the parts will be equally well suited to traditional 5V as well as ultra-portable battery applications with its 1uA typical current draw helping to reduce energy consumption. Powered down, the devices' output circuitry is automatically disabled to prevent damaging backflow current and to ensure signal isolation. With 5.5V tolerant inputs, the logic products can also serve as voltage translation devices. Further information is available at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Dallas, Texas. Design, marketing, and engineering centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
972-385-2810
pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
949-224-3874
lsievers@sheltongroup.com