Diodes Menu Close

Press Releases

Press Release

Back to Press Room

Compact Linear LED Driver from Diodes Incorporated Suits Low-Current Lighting Systems

Sep 12, 2012

PLANO, Texas--(BUSINESS WIRE)--Sep. 12, 2012-- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today announced the AL5812 60V linear LED driver. The AL5812 delivers a constant current of up to 150mA and provides designers of low-current illumination and signage applications with a simplified circuit solution for accurately controlling 1/2W LEDs. Housed in a small-footprint, thermally enhanced SM package option, the driver is able to meet power handling requirements over a wide supply voltage and ambient temperature range.

LED current is set using a high value resistor on the driver’s low voltage, 0.5V RSET pin, enabling the specification of a lower cost, smaller footprint resistor to reduce total system BOM cost. A standard low-value decoupling capacitor is the only other external component needed. The driver maintains an LED current accuracy to a tolerance of 3%.

Offered in the exposed pad MSOP-8EP and U-DFN3030-6 packages, the AL5812 drives up to 16 low-power LEDs, with its open-drain output handling a swing from 1V to 60V. The driver’s industrial temperature range of -40ºC to +125ºC means it readily accommodates high luminaire operating temperatures. For further information, visit the Company’s website at www.diodes.com.

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and two joint venture facilities located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Fort Worth, Texas; Taipei; Hong Kong; Manchester; and Munich, Germany, with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.

 

Source: Diodes Incorporated

Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-987-3900
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com